12/19/2018 2:46 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32890 Rating: (4066)
|
In the attachment a possible solution. Every 15 minutes, the current actual value is compared with the stored value. If the values are different, an action can be triggered via B007. B007 is also responsible for saving the current actual value as an old value. AttachmentAnalog_monitoring-0BA8.Standard.zip (173 Downloads) |
12/19/2018 2:56 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
To calculate ds/dt you can use MaxMin as shown in the attachment. They can be cascaded with analog markers, if you need several values. In the second line you see some comparators as example. I don't know, what you want to compare. Look also to the Analog watchdog. This special function saves the process variable of an analog input to memory, and sets the output when the output variable exceeds or drops below this stored value plus a configurable offset. Maybe the program can show you the right direction to a solution. Regards, Scorp AttachmentDeltaS_DeltaT.zip (162 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on