12/20/2018 12:54 PM | |
Joined: 6/4/2010 Last visit: 5/10/2024 Posts: 376 Rating: (126)
|
Dear forum member, The Desigo Insight Management Station provides backward compatibility only. This means that e.g. Desigo Insight V5.1 supports all the old controller versions (V2.37, V4.0, …, but not the newer versions (V6.0). The only exception to the above statement is the Desigo Insight V5.1 Servicepack 2 with Hotfix H39. Installing Hotfix H39 allows to support the Desigo PX controller firmware V6.0 and DRA V1.2. Please see in the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/109480767 (For the ones with Extranet or Intranet access only.) Please note that even though the above Hotfix provides the BACnet compatibility, the new Desigo PX compounds are not supported by the DI graphic library. Other restriction may apply. Please note that the Desigo Insight V5.1 Servicepack 2 has been released nearly 5 years ago. It does not support the current Microsoft operating systems nor the latest Desigo Room Automation versions. It may be wise to upgrade the installation to the current Desigo Insight V6.0 SP3 anyway, to ensure a secure, stable and reliable operation for the next years. A migration to the Desigo CC may be an other option. Best regards, Albis |
This contribution was helpful to2 thankful Users |
Follow us on