12/29/2018 4:54 AM | |
Joined: 8/25/2006 Last visit: 9/24/2024 Posts: 2209 Rating: (278)
|
Hello. o10.0 means that the OFF2 command is input to the drive via binector (P655, P656 or P657). OFF2 - voltage disconnection, switching on the drive is inhibited, drive is not ready. When the drive is ready for switch on you should get on the PMU o7.0 or o7.1, after switching on the drive you should get the higher state on the PMU - o6.x, o5.x,..., o1.x, I II --. Look for description of r000 in the manual. |
Follow us on