1/2/2019 9:40 AM | |
Joined: 10/11/2006 Last visit: 4/22/2024 Posts: 5820 Rating: (789)
|
Hello, the old encoder was 2048 sin/cos (22Bit) + 4096 Multiturn (E). The new one is only 20Bit Sibgleturn (Q). When at the Simotion TO (Technology object) data adaption is activated, you have to do nothing. You can check the settings for the 20Bit singleturn. Encoder pulses per rev: 512 (P408) Fine resolution: 2048 (P418) Fine resolution of absolute value Gn_XIT2: 512 (P419) Data width of absolute value without fine resolution: 9 and you can check the "Reference Variables". TO Axis Electric / Hydraulic, External Encoder 3.4.4 Setting as a real axis with digital drive coupling https://support.industry.siemens.com/cs/ww/en/view/109757317 |
With best regards, |
|
Follow us on