1/1/2019 4:34 AM | |
Joined: 3/30/2014 Last visit: 3/31/2024 Posts: 75 Rating: (3) |
Hi,I am having trouble using SIMOTION D445-2 to perform Profinet communication configuration with KUKA .SIMOTION Firmware(Kemel) is V4.5 or V5.1. If I use V4.4,there is no problem at all. KUKA GSDML file be found in the attachment . AttachmentKUKA_GSDML.zip (184 Downloads) |
1/1/2019 4:38 AM | |
Joined: 3/30/2014 Last visit: 3/31/2024 Posts: 75 Rating: (3) |
This is the problem: |
1/7/2019 10:56 AM | |
Joined: 10/11/2006 Last visit: 5/3/2024 Posts: 5832 Rating: (790)
|
Hello following your enquiry I add both GSD-Files on SIMOTION Device V5.1 (attached screens) It seems well AttachmentKuka_screens.pdf (140 Downloads) |
With best regards, |
|
Follow us on