1/10/2019 10:34 AM | |
Posts: 7 Rating: (0) |
Hello PS: Thank you for replying ------------------------------------------------------------------------------------------ AttachmentDiag.zip (184 Downloads) |
Last edited by: Jen_Moderator at: 1/10/2019 11:35:40 AMNew subject after splitting |
|
1/10/2019 12:47 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi Mihal33, try a repair-installation, or better, install the latest Update for V14 SP1. Updates für STEP 7 V14 SP1 und WinCC V14 SP1 Do the installation with deactivated anti-virus-scan and as admin(right-click on Setup.exe->run as admin) hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
1/10/2019 2:46 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
Are you running win10? If so, what build, and do you know which win10 builds v14 sp1 states are supported? Have you ever been able to go online with this computer and tia portal since installing V14 SP1 update 5? If you have been able to go online with portal in the past, I 100% agree with the repair of the TIA Portal install/ You might even consider installing the latest V14 SP1 update. I see updates 6 & 7 available. One of them might fix the problem.
|
science guy |
|
1/14/2019 5:26 PM | |
Posts: 7 Rating: (0) |
thank you for your reply Already installed update 7, but didn't helped. I think, probably it is port or some service problem in computer. |
1/14/2019 5:37 PM | |
Posts: 7 Rating: (0) |
THX for replaying. Yes it is 1607 win 10 build (V14 - No W10, V14 SP1 old till - 1703 build if I remember, V15 - all builds). TIA was OK till the holidays (whole year 2018). The pc is in clients facility and its serves as VPN work station. No update was installed and I can ping all the devices in the network. The only problem is when I click on the go online (download, upload, so on...) its automaticly crash, (even extended go online = crash, no popup window). When I was checking the diagnostic files there was only massage: unhandled, so I dont have info about the problem. Thats why I asking :(
|
Follow us on