Industry Online Support
Technical Forum
1/15/2019 10:40 PM | |
Joined: 10/31/2005 Last visit: 9/4/2024 Posts: 366 Rating: (31) |
I hope you'll be able to help me with the following problem. I have S7400 PLC (CPU 412PN) that is via Port 2 connected to Port 1 of Scalance x101-1 media convertor, ord. nr. 6GK5101-1BB00-2AA3. Then I have FO network (more than 300 m in length) to the Scalance X204-2 switch. Port 2 of X101 is connected to port 5 (FO port) of Scalance x204-2. On ports 1 and 2 (RJ45 204-2) are connected two ET200M (IM153) modules. Topology is shown in the attached pictures. When I try to save and compile this I get error message that Cable IDs are different. Error mesage is also attached. I have tried to find scalance x101 in HW catalog in Netpro and in HW Config but cannot find it. Scalance x101 media convertor is visibile only in topology. Do you have any advice how to solve this problem? Thank you!
Attachmentnetwork.zip (52 Downloads) |
Last edited by: Pandiani at: 1/15/2019 10:46:15 PM |
|
1/24/2019 9:59 PM | |
Joined: 10/31/2005 Last visit: 9/4/2024 Posts: 366 Rating: (31) |
Hello Murof, I use STEP 7 v 5.5. |
Follow us on