1/18/2019 10:52 PM | |
Posts: 25 Rating: (0) |
Hi, I have connected a HMI Exor to the PLC LOGO V8 How can i Digital & analog network input Function values (vm) persistent memory when the logo is restarted |
1/19/2019 6:31 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32889 Rating: (4066)
|
The VM memory of the LOGO! is not retentive. The HMI transmits the signals to the VM memory only once, namely at the time of acceptance of the value. If the LOGO! restart, the VM memory is empty. With the digital values you work best with pulse signals (like a button, not like switches) and in the LOGO! with latchuing relay or pulse relay. AttachmentForum.zip (121 Downloads) |
1/19/2019 10:51 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32889 Rating: (4066)
|
I can not say without having seen the program. In any case, the VM memory of the LOGO! not retentive. |
1/19/2019 11:40 AM | |
Posts: 25 Rating: (0) |
this progaram |
Follow us on