1/31/2019 2:26 AM | |
Posts: 80 Rating: (1) |
Hi All, Is there any profibus coupler for S7-400 racks? Best regards Azad |
1/31/2019 2:52 AM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello Azad; There are no Profibus slave IMs for S7-400 racks, such as exists for the S7-300/ET 200M (IM 153-2) or ET 200S (IM 151-1). The only way to use a S7-400 rack in an expansion configuration is shown in the screenshot below, extacted from the S7-400 Module data manual, chapter 6, Interface Modules: https://support.industry.siemens.com/cs/ww/en/view/1117740 You could also look at the contents of this discussion, from another automation forum: http://forums.mrplc.com/index.php?/topic/13729-s7-400-dp-slave-module/ Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/31/2019 3:27:13 AMLast edited by: dchartier at: 1/31/2019 12:20:36 PM |
|
Follow us on