2/8/2019 5:02 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32887 Rating: (4066)
|
Personally, there are no abnormalities noticed. |
2/8/2019 5:07 PM | |
Posts: 29 Rating: (0) |
interesting as I have not done that many projects yet and seen it multiple times :D |
2/8/2019 5:16 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32887 Rating: (4066)
|
Then start a Support Request. Give exact details: |
This contribution was helpful to1 thankful Users |
2/14/2019 8:49 PM | |
Posts: 51 Rating: (5) |
I think that maybe i understood the problem, if so it is not a BUG but a program mistake. For a few blocks you want to use a inverted input to "cheat" and activate the block like msg. text or timer, for other blocks this cheat will not work because the program is not compleet. If you want to call it a BUG, it is only because the self test does not pickup your mistake. see the attachement Boo4 will never work this because input 2 is inverted but not connected. for the timer and text block this is not a problem. I hoop this is what you see and explain the problem/solution. Attachmentinverted input failure.zip (65 Downloads) |
Follow us on