2/22/2019 4:29 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
Hi, have you tried using the Information System/help feature within the TIA Portal (F1) in order to know in detail about the forcing? You may use the attachment here as guidance to locate the same contents within the TIA Portal in your machine. AttachmentForcing IO.zip (177 Downloads) |
2/22/2019 2:00 PM | |
Joined: 12/7/2011 Last visit: 4/29/2024 Posts: 384 Rating: (9) |
Im not able to force single digital input or output . Are we sure that does not exists any limitation fro S7 400 Cpu with Tia portal? Furthermore in the help files, i found this sentence: "If the function Enable Periheral Output is active on your cpu,forcing is not possible. If desired, deactive this function in wacth table . What kind of function is? I didn't found any "Enable Periheral Output" into the wacth table, anyone knows? Ragards. Duccio. AttachmentForcing.pdf (130 Downloads) |
Last edited by: Duccio at: 2/22/2019 2:01:52 PM |
|
2/25/2019 1:39 AM | |
Joined: 2/20/2014 Last visit: 4/25/2024 Posts: 395 Rating: (38) |
Hi Duccio, Can you create a file (program file) with the hardware & list of address that you wish to force? If you do not wish to upload the program file with your actual logic (can you create a simple file for testing the forcing of the IO points?). |
2/25/2019 7:16 AM | |
Joined: 12/7/2011 Last visit: 4/29/2024 Posts: 384 Rating: (9) |
Ok, today i will. Thanks for the support. Duccio. |
2/27/2019 10:13 PM | |
Joined: 9/21/2012 Last visit: 5/6/2024 Posts: 3937 Rating: (444) |
In Dropbox, you can create a download link from the uploaded file. Then you can share the link here. |
2/28/2019 9:22 PM | |
Joined: 12/7/2011 Last visit: 4/29/2024 Posts: 384 Rating: (9) |
Hi guys, here's the link to download the project. https://www.dropbox.com/s/wdgynopxf5et9vy/TiaProject.zap14?dl=0 Im not able to force any boolean DI or DO, only byte word o dword. Please, let me know any news. Thanks. Regards. Duccio. |
3/11/2019 11:32 AM | |
Joined: 12/7/2011 Last visit: 4/29/2024 Posts: 384 Rating: (9) |
HI guys. No one suggest? |
Last edited by: Duccio at: 3/11/2019 11:33:10 AM |
|
Follow us on