3/11/2019 4:52 PM | |
Posts: 1 Rating: (0) |
Hi , All the signal assignments to System interface are deleted . I need to configure the CB & Disconnect status to Unassigned Byte & Bit. (0/0 & 0/1 ..) as per the DCS signal list. While mapping in Signal Matrix 4.93V , I cant see Byte - 0 & Bit from 0 to 7 , which shall be user defined as per the manual . Please see the attachments for screen shots Please help me ------------------------------------------------------------------------------------------ AttachmentSignal Mapping for Profibus 3-1.zip (66 Downloads) |
Last edited by: Jen_Moderator at: 3/12/2019 10:42:33 AMNew subject after splitting |
|
Follow us on