3/17/2019 5:52 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
hi, need some help with part of the attached program if possible. I would like machine stop part of the program to flash amber when input 5 is active and take priority in preference to screen 10 and return back to screen 11 once i5 is deactivated. many thanks Attachmentspeed_m_c_stops_line1.zip (136 Downloads) |
3/17/2019 6:06 PM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
Like so as in attachment?
Attachmentspeed_m_c_stops_line1_V2.zip (147 Downloads) |
3/17/2019 6:38 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Thank you so much |
3/17/2019 6:40 PM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
You're welcome... Is your problem solved? |
3/17/2019 10:09 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
problem is solved |
3/18/2019 6:48 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hi, I seem to be going round in circles,would appreciate some suggestions... I would like to better utilise input 2 and remove input 5 from the program(see attached) so input 2 line active machine status running....input 2 not active amber alarm page displayed and counting. Attachmentspeed_m_c_stops_line1_V3.zip (142 Downloads) |
3/18/2019 7:07 AM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
And where is your problem? Do not understand your question.... |
Follow us on