12/27/2010 12:43 PM | |
Joined: 9/23/2005 Last visit: 9/25/2024 Posts: 4347 Rating: (1446)
|
Hi, Follow I attached a sample program with a PID and a field simulation (STEP 7 V10.5). With this field simulation it is possible to see how the PID self tunning works, without a phisical installation associated. In the follow post (2013/01/07) I place a new version, for V11, that includes an additional test logic for set mode =3 / automatic reset the PID. See also the TIP for PID (PID Compact) at /tf/WW/en/Posts/33957 AttachmentPID with Field Simulation.zip (4231 Downloads) |
Last edited by: Pegaia at: 1/7/2013 12:00 PMLast edited by: Pegaia at: 1/7/2013 11:50 AMDenilson Pegaia |
|
This contribution was helpful to3 thankful Users |
7/21/2012 11:20 PM | |
Posts: 1 Rating: (0) |
not being stupid but how do you u use it or open it? thanks
|
8/11/2012 9:16 AM | |
Posts: 21 Rating: (1) |
it could not possible to open it in step 7 v 5.4 or some other file which could be open in step 7 v5.4 |
8/13/2012 12:21 PM | |
Joined: 9/23/2005 Last visit: 9/25/2024 Posts: 4347 Rating: (1446)
|
Hi, this sample was created for V10/V11 STEP 7 versions. It couldn't be opened by V5.x. Here there is a printout of the example. So you can convert it to any other system. AttachmentE:\to PG\document.zip (1548 Downloads) |
Last edited by: Pegaia at: 1/7/2013 11:47 AMLast edited by: Pegaia at: 8/13/2012 12:33 PMDenilson Pegaia |
|
1/7/2013 12:05 PM | |
Joined: 9/23/2005 Last visit: 9/25/2024 Posts: 4347 Rating: (1446)
|
Hi, Follow I attached a sample program with a PID and a field simulation (STEP 7 V11). With this field simulation it is possible to see how the PID self tunning works, without a phisical installation associated.This includes an additional test logic for set mode =3 / automatic reset the PID. See also the TIP for PID (PID Compact) at /tf/WW/en/Posts/33957 AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\Sample PID V11.zip (1804 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
6/21/2016 5:30 PM | |
Posts: 21 Rating: (0) |
can you do video this it? |
10/23/2018 3:13 PM | |
Joined: 10/22/2018 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
Hi, First, congratulations for your work. Ishould need this sample in a version 15. Tank you. |
3/24/2019 9:34 AM | |
Joined: 6/5/2018 Last visit: 7/24/2024 Posts: 44 Rating: (0) |
HI Unfortunately i have TIA Portal V15 Latest Update and cant open it :( i dont have TIA Portal V13 Or older versions ... can every one help me? |
12/4/2019 10:18 AM | |
Posts: 1 Rating: (0) |
Hi |
Follow us on