3/24/2019 11:17 AM | |
Joined: 8/5/2017 Last visit: 3/17/2024 Posts: 4 Rating: (0) |
Hi; Can you help me ? How can i run this code?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/25/2019 1:08:18 PMNew subject after splitting |
|
3/25/2019 4:19 PM | |
Joined: 8/3/2009 Last visit: 4/19/2024 Posts: 12816 Rating: (1634)
|
Hello there are a few errors in it. for example in the "if" statement you use a = this is in C Script an assignment not a comparisson. so if you want to check if its euqal then use == or <= or < or something else.. The Tag_1 is not declared. Is this a global C Script Tag? IF not use the GetTagXXX Functions to read out. the for Statement is not the correct syntax you have to write for(i=1;i<5;++i) for example. And so on. ??? you will never get this script though the compiler. so do you have experience in using C Programming? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on