4/1/2019 7:06 AM | |
Joined: 10/27/2016 Last visit: 12/27/2022 Posts: 4 Rating: (0) |
Hi, We are facing similar problem currently. We were having problem with external encoder system and we bypassed the same and were running the machine with motor encoder from last 2months but from last few days we were having problem with servo motor so we changed servo motor and run machine. it run for sometime and we are facing problem with same alarm. we tried increasing 36942 36944. and change 36901 and temporary running machine. alarm fault is coming but axis is running. I am unable to understand as it was running smooth before with motor encoder. 27001 is getting generated with NC command given and drive is not updating alarm with single encoder and triggering alarm? is it difference between axis MD parameter vs Drive Md parameter? How did you resolve the issue when you faced this issue? ------------------------------------------------------------------------------------------ |
Last edited by: Harsh201 at: 4/1/2019 7:08:01 AMLast edited by: Jen_Moderator at: 4/2/2019 9:32:47 AMNew subject after splitting |
|
Follow us on