2/12/2019 9:01 AM | |
Joined: 9/22/2017 Last visit: 6/27/2024 Posts: 1 Rating: (0) |
Hello smiffy, Could you tell me how to access larger DB addresses using pAny.ByteAddressMSB please? Thank you, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/12/2019 1:45:35 PMNew subject after splitting |
|
4/9/2019 4:43 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello sagark, I recommend to use the following FAQs (see links) for creating the ANY pointer. Then you can transfer the data from one DB to the next DB. How can you calculate an offset for an ANY pointer or change the pointer? How do you program the ANY parameters for SFC14 and SFC15 in S7-SCL? How do you parameterize blocks, which have "ANY"-type or "Pointer" type parameters? Cicero |
4/10/2019 9:24 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi Fennar, You can use SFC19 BLK_MOV for accessing larger amount of data. The question is really not understood -What do you mean by larger DB area access. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on