4/9/2019 7:45 PM | |
Posts: 8 Rating: (0) |
dear Christoph hi I have a same problem like Antri with my Wincc V7.4 sp1 to install on Windows 7 ( i tried all versions (32Bit & 64Bit) (Pro & Ultimate)), while installing the wincc V7.4 with "SQL Server 2014 Standard Edition (Wincc) Setup cannot complete the installation" error stops and it dosnot install. I check my username that it dosn't have any blank in it. also before this i have installed this wincc (V7.4 sp1) with this source on another system without any problem. would you help me to solve this problem?? ------------------------------------------------------------------------------------------ |
Last edited by: ehsanbank at: 4/9/2019 7:46:05 PMLast edited by: ehsanbank at: 4/9/2019 7:50:06 PMLast edited by: ehsanbank at: 4/9/2019 7:51:24 PMLast edited by: Jen_Moderator at: 4/10/2019 11:22:36 AMNew subject after splitting |
|
4/10/2019 11:23 AM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8026 Rating: (163) |
Closed cause question posted twice. The second thread with the subject SQL server Standard edition error while installing Wincc V7.4 is published within the conference SIMATIC WinCC.
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on