4/10/2019 2:35 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi Can you show the code that doesn´t work? Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/10/2019 8:26 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi Righ know , I don´t have open WinCC so I will tell you the code with VBScript
With ANSI-C, you have to change the value of your properties, search:
Regards
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/12/2019 9:24 AM | |
Posts: 5 Rating: (0) |
AttachmentCapture1.zip (43 Downloads) |
4/12/2019 12:16 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi I saw your screenshots: 1.- With VBScript there is an error, because "x" don´t exist, you must change x with a value or define
2.- With ANSI-C , you are making a mistake, because you are in the same property. so it is not the ritgh place to call SetPropXX(Parameters) Where you are in the screenshots, you must return the value directly. The right place to call SetPropXXX is when you press a button and you change the picture windows and you move the triangle. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on