4/15/2019 4:17 PM | |
Posts: 9 Rating: (0) |
Hello Pigroplc, When I open the SW with STEP7, the error-window does not appear, but never happens on the SW. Please see the attached file. Important to mention that I tested this issue with 4 other SW's project and the behavior is the same, i.e., I can open them normally in my "old" laptop and none SW can be open in the "new" latpot. It is not a problem with a specific SW's project. Thanks, Jorge AttachmentSTEP7.pdf (193 Downloads) |
4/15/2019 4:22 PM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22221 Rating: (2979)
|
Hello, the last screen looks not ok. Do you have installed all latest Windows Updates? Regards Christoph |
4/15/2019 6:44 PM | |
Posts: 9 Rating: (0) |
Hello, None all of them, 3 updates are not possible due to erros during the updates: KB2773072 KB3159398 KB2931356 Regards, Jorge |
4/16/2019 2:26 PM | |
Posts: 9 Rating: (0) |
Hello pigroplc, I proceeded acc. to your recomendation and it didn' work, unfortunately! Regards, Jorge |
4/16/2019 4:23 PM | |
Joined: 4/3/2008 Last visit: 4/22/2024 Posts: 385 Rating: (16) |
Jorge, can you open an S7-300 project with this damned laptop flawless or do you face some issue either? pigroplc |
Follow us on