4/18/2019 6:42 AM | |
Joined: 5/1/2013 Last visit: 3/29/2024 Posts: 426 Rating: (3) |
Hello If I call FUNCTION BLOCK multiple times, do I have to create each different instance DB? Thank you. |
4/19/2019 2:54 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi RetroK, Yes. U will need to assign diffrent IDBs for every call. FB is code. IDB is specific for each individual element. So diffrent IDBs. U can also create Multiple instance & club all data in single IDB. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on