4/15/2019 6:29 PM | |
Posts: 5 Rating: (0) |
i seem to have a more basic problem in that I am unable to change MD10240. It is greyed out and the Settings page indicates 'Current access level: User'. Could you please let me know how I can change the access level so I can change 10240? I am running Sinutrain 4.8 SP4 on Win 10 64 bit with the DEMO-Lathe machine and the basic license.Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/16/2019 11:20:27 AMNew subject after splitting |
|
4/18/2019 10:39 AM | |
Posts: 2964 Rating: (478)
|
hello, you need to change the access level to expert mode / machine manufacturer. you can check the access level and do accordingly. Attachmentaccess level.pdf (172 Downloads) |
4/19/2019 9:45 AM | |
Joined: 4/28/2015 Last visit: 4/24/2024 Posts: 320 Rating: (35) |
Hi The same process can be followed within Sinutrain, I am guessing you are using the Solutionline version of Sinutrain and not an older Powerline variant? Menu Select > Setup > Password > Set Password MD10240 = 1 - Metric System MD10240 = 0 Imperial System I have just performed this on Sinutrain v4.7 and works ok Hope this helps Luke |
Last edited by: Luke_N at: 4/19/2019 9:45:45 AM |
|
This contribution was helpful to2 thankful Users |
4/24/2019 4:31 AM | |
Posts: 2964 Rating: (478)
|
Hello, Mr.Luke is right basic switch over softkey is visible. i had checked also and it is there.
Attachment10240.pdf (105 Downloads) |
Follow us on