4/18/2019 8:39 AM | |
Joined: 5/20/2016 Last visit: 7/7/2023 Posts: 32 Rating: (0) |
i working in 5axis machine with 840Dsl control and S120 drive , all things ist ok but in MDI ,i dont can run any command. i have "700761" error AFTER press cycle start button. i know this error ist DB2.DBX243.5 in plc, i have complete plc program in SIMATIC Manager, but when i search DB2.DBX243.5 ,dont can find it i attached plc program any idea ? Attachment840dsl_p.zip (57 Downloads) |
4/18/2019 10:53 AM | |
Joined: 5/20/2016 Last visit: 7/7/2023 Posts: 32 Rating: (0) |
thx for reply but i am sure that 700761 ist DB2.DBX243.5 please see picture |
4/21/2019 9:07 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Please check HHU unit connected via Ethernet, if station clamping/declamping signal/selection is wrong on the HHU. It is OM as correctly pointed out/mentioned by forum member CNC600 HTH |
Follow us on