4/22/2019 2:41 PM | |
Joined: 3/10/2016 Last visit: 6/5/2024 Posts: 3 Rating: (0) |
Hello. I have When I run motor identification, I get an error: 7982 : Drive: Rotating measurement encoder test(7) p0408=1024 The values of r479 r482 (actual position) per one revolution are 2 ^ 21 (1024 * 2048). It is not clear to me why not 1024. Counting working right? I understand that I receive the wrong number of pulses from the encoder. I can not find an error. What could be the problem? [snip] Thank you. P.S. I read https://support.industry.siemens.com/tf/WW/en/posts/drive-commissioning-error/20537?page=0&pageSize=10 AttachmentFiles.zip (232 Downloads) |
Last edited by: AutoGen_8539125 at: 4/22/2019 2:43:19 PMLast edited by: Jen_Moderator at: 4/24/2019 7:28:43 AMRemoved links and added files as an attachment. |
|
4/22/2019 3:55 PM | |
Joined: 7/7/2010 Last visit: 9/19/2024 Posts: 15207 Rating: (2417) |
In the configuration, temporarily change the control / feedback strategy from <whatever> + encoder to <whatever> + encoderless. Commission as much as you can without the encoder for feedback. The encoder A/B direction could be reversed. You can adjust it in drive configuration using Drive Navigater -> Encoder and invert the encoder signal. Or, you can swap A/-A & B/-B (and Z/-Z). Turn the shaft one revolution, or as close as you can to one revolution. Monitor the encoder raw input and calculate the difference in pulses. If you have approximately the correct PPR for the encoder configuration (quadrature or single channel for example), the wiring and encoder are ok. If there is something wrong with the count or it seems to count strangely, verify the wiring, maybe even using an o-scope.
|
Last edited by: Jen_Moderator at: 4/24/2019 7:29:20 AMRemoved links. science guy |
|
5/1/2019 3:00 PM | |
Joined: 3/10/2016 Last visit: 6/5/2024 Posts: 3 Rating: (0) |
I think it might come in handy.
|
Last edited by: AlxndrBo at: 05/01/2019 15:03:16Last edited by: AlxndrBo at: 05/01/2019 15:04:50Last edited by: Jen_Moderator at: 05/02/2019 11:32:17Optimized link. |
|
Follow us on