4/17/2019 4:05 PM | |
Joined: 7/6/2016 Last visit: 2/6/2024 Posts: 3 Rating: (0) |
Hi All Has anybody tried to use the Schneider Electric Lexium LMD motor using a S7-300 PLC in TIA v14 or v15? Schneider provide the LAM_DB and Data-types: https://motion.schneider-electric.com/dloads/automation-libraries/ However, this is not compatible with the S7-300. "Optimized Block Access is not supported". Has anybody created a similar block to control these motors? I have set-up the motor using the Schneider Lexium MDrive software and I can go online to the motor within TIA. The PLC Open libraries in the link below do not work within TIA, only Step7. https://www.schneider-electric.ie/en/download/search/SE_Motion_LXM32_S7_V1005/ |
4/17/2019 7:33 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
You can modify the DBs / FBs to not require optimized block access and adjust the blocks to work correctly for S7-300's.
|
science guy |
|
4/18/2019 4:31 PM | |
Joined: 7/6/2016 Last visit: 2/6/2024 Posts: 3 Rating: (0) |
Hi huggy_d1, thanks for the response, I am unable to as I do not have the Attributes page in the DB Properties (it is greyed out), see attachment. I have set the Protection properties in the PLC to 'No protection'. Regards James AttachmentLAM FB250 properties.docx (71 Downloads) |
1/14/2021 9:55 PM |
|
Joined: 1/12/2011 Last visit: 9/10/2024 Posts: 59 Rating: (5) |
Terrible block. |
Follow us on