4/22/2019 12:02 PM | |
Posts: 2 Rating: (0) |
Greetings people, I am currently trying to make communication between Scalance W774 (along S7-1500) as Access Point and Scalance W722 (along S7-ET-200-SP) as the Client. I am using the TIA Portal V15. I am failing in establishing communication. Please also point out where the Siemens documentation recommends client modules for the Access Points. Note: The Key plug being used is W780. I used the Primary Setup Tool to configure both the Access Point and the Client module. I was earlier doubtful that W774 would perhaps not be suitable for communicating with W722. But as Gabbar mentioned in this thread, that he has successfully established communication, my doubt has now shifted towards the key plug. The key plug i have available is 6GK5907-8PA00 \ KEY-PLUG W780 IFEATURES. ------------------------------------------------------------------------------------------ |
Last edited by: furqankaimkhani at: 4/22/2019 12:09:24 PMLast edited by: Jen_Moderator at: 4/22/2019 1:44:59 PMNew subject after splitting |
|
Follow us on