5/30/2019 6:19 PM | |
Posts: 1 Rating: (0) |
I create a connection with AI in NOD-RED (in the picture). Read - once a second. At the output, in debug , in the absence of an input signal, values from 140 to 143 (in the picture) appear. Where do these values come from? I connect the KCT-10, 60A / 20mA current sensor to AI IoT 2040. The fluctuations of the values increase, the amplitude is about 30–150, with the load current in the primary circuit being 8.35A. How does the ADC work in this mode? AttachmentPictures.docx (142 Downloads) |
Last edited by: mzh_99 at: 05/30/2019 18:21:15 |
|
Follow us on