5/31/2019 11:02 PM | |
Joined: 8/17/2017 Last visit: 12/18/2023 Posts: 3 Rating: (0) |
Hello, I would need to know if, when I buy a powerblock, the IPD card corresponding to that powerblock is included or if it has to be purchased separately. If it is necessary to acquire it separately there is a catalog to know which IPD card corresponds to which powerblock? (infeed, motor, etc) Regards ------------------------------------------------------------------------------------------ |
Last edited by: nicolasguanzini at: 05/31/2019 23:51:49Last edited by: Jen_Moderator at: 06/03/2019 10:41:24New subject after splitting |
|
6/1/2019 7:14 AM | |
Posts: 153 Rating: (7) |
When you order only power block its just a spare so ipd will not be included. But if you order full power module means full drive then it will be included based on your name plate and MLFB. You can go to spares on web ( https://www.sow.siemens.com) and type your MLFB and serial no. You will full spares list which can be used for the specified product. You can not use the any IPD it should be based on your drive rating.
|
6/14/2019 12:59 AM | |
Joined: 8/17/2017 Last visit: 12/18/2023 Posts: 3 Rating: (0) |
Thank you very much, it has been very helpful. I have another question about the Power Blocks. Currently we have four different "types" of modules in the factory. Some are motor modules that are composed of a single Power Block. Others are composed of 3 power blocks The same for the infeed. We have some Smart infeed composed of 3 power blocks and others with 1 powerblock. The question is whether in the case of the modules composed of 3 power blocks each block corresponds to a single phase of the motor in case of the motor modules, or if the 3 blocks work in parallel (I attach a drawing of how I "believe" the circuitcan be) The same question for the infeed, each power block corresponds to a single phase? Can you share a diagram of how the IGBTs are arranged in the infeed and the motor modules? Here a link to a picture of how the cabinets look and also give them the code of the powerblocks Link image Cabinet module Power block 735A Motor module: 6SL3352-1AG37-4FA1 Power Block 1200A Smart Infeed: 6SL3353-1AG41-2FA0 Regards Attachmentfiles.zip (119 Downloads) |
Last edited by: Jen_Moderator at: 06/17/2019 06:09:01Removed link and added files as an attachment. |
|
Follow us on