11/4/2019 4:05 PM | |
Joined: 11/29/2011 Last visit: 9/24/2024 Posts: 1359 Rating: (232) |
Hi, So I have a set up for one PCS7 ES, 3 Engineering Client running on V7.1 no Service Packs. Based on SIMATIC PCS 7 Virtualization for V7.1 SP2 the HP Blade System “C7000 Enclosure G2” would do. I suppose the V7.1 without SP's would run just as well. Finding VM's with Server2003 will be still a challange. Based on the bellow drawings could you put in direction to locate appropriate Server? Also source of VMs with Preinstalled PCS7 V7.1 or fresh Win2003 installation? This feels a bit hopeless. Maybe I have to tell my client to migrate or pull the plug... |
Last edited by: MicroMan at: 11/04/2019 16:06:11- What you read here, please check with manuals and your requirements. |
|
Follow us on