3/4/2020 10:57 AM | |
Joined: 2/10/2017 Last visit: 10/10/2023 Posts: 53 Rating: (1) |
Looks like it doesn't work with Image 2.6 I try to copy it to /usr/lib/node_modules, and install it. However, node doesn't appear in Node-red. I also try to copy it to /home/root/.node-red/node_modules, and install it. Nothing appears in Node-red as well. It used to be fine in Image V2.4, but looks like not for V2.6. Does it mean that I can use Intel GPIO without any problem with Image V2.6 now? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/04/2020 14:49:56New subject after splitting |
|
3/4/2020 3:02 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
An enhanced version of node-red-node-intel-gpio is pre-installed on the images, 2.6 as well as older versions. It works as-is. However, the installation path and version chosen for 2.6 had an unwanted side-effect on the deinstallation of other node-red nodes. This is addressed by |
Follow us on