4/17/2020 9:14 AM | |
Joined: 7/5/2017 Last visit: 3/11/2024 Posts: 5 Rating: (0) |
Hi, Yesterday I had a PLC going into stop, and the reason why is not clear for me. In the diagnostic buffer (in atachment) I found event 147 Maintenance demanded: Safety program: Warning limit cycle time exceeded Event ID: 16# 0D:75ED event 146 Error: PROFIsafe communication failure (timeout) Event ID: 16# 08:0318 event 145 Temporary CPU error: Maximum program cycle time exceeded Event ID: 16# 02:3501 What is the real cause of the CPU would it come from the safety or from the standard program? CPU is 1516F-3 PN/DP firmware V2.6.1 Kind regards, AttachmentDiagnostics1516F.txt (279 Downloads) |
4/20/2020 8:34 AM | |
Joined: 7/5/2017 Last visit: 3/11/2024 Posts: 5 Rating: (0) |
there are no loops programmed in the safety program |
Follow us on