4/17/2020 6:16 AM | |
Joined: 7/14/2016 Last visit: 9/12/2023 Posts: 387 Rating: (27) |
Hello, Sorry for opening old thread but I find it very frustrating that latest software from Siemens is not supporting latest OS. Microsoft is not providing enterprise version 2015 LTSC in my region. It is old OS now. I am helpless now, what to do? Is siemens offering any IPC suitable as ES and OS for PCS7 v9.0 SP2? Is any of this suitable? Kbv. |
Last edited by: Kbv at: 04/17/2020 06:19:16Don't just think in terms of solutions... |
|
4/17/2020 7:48 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi Kbv, I understand your frustration. LTSC 2016 is also not supported, but maybe Microsoft Server 2016 x64 bit is suitable for your case? I don't know if this is available to you as well? This year PCS7 V9.1 should be released on the market. Maybe this version supports Windows 10... we have to wait for more details. |
If I could help you, you can use the RATE button. Thank you. |
|
8/28/2020 8:43 AM | |
Joined: 3/20/2019 Last visit: 10/12/2023 Posts: 6 Rating: (0) |
this problem is solved after reinstalling the software |
This contribution was helpful to1 thankful Users |
Follow us on