9/3/2020 8:37 AM | |
Joined: 9/2/2020 Last visit: 2/6/2024 Posts: 2 Rating: (0) |
Hi, the tia portal is a sw for create a project to download inside to PLC . In tia portal we can program both the software for the plc (in various languages --- SCL, AWL, LAD ...) we have as the old step7 the HW configuration for the various devices connected to the PLC. In addition we can also program an HMI interface. The positive side of the tia portal is that we have a high-level language and we can refer to our "objects" with nomenclature, and tia them even in complex structures. You can find a lot of tutorial for develop in tia portal with scl lenguage (my favorite lenguage :D) . ***** exsemple tutorial link : https://www.youtube.com/watch?v=tpLNRPR9MPU **** |
Last edited by: Jen_Moderator at: 09/03/2020 10:16:46Embedded video. kinds Regards |
|
9/3/2020 11:48 AM | |
Joined: 9/21/2012 Last visit: 4/19/2024 Posts: 3911 Rating: (443) |
TIA Portal is software you can use for PLC, HMI and SCADA. |
9/3/2020 12:07 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi together, TIA-Portal is the framework for the engineering SW packages. Here are the major contents of TIA: WinCC is for HMI. There are different versions, like Basic, Comfort, Advanced. WinCCprofessional is for Scada-Systems. Step7 is for programming, there are also different versions and packages. Basic is only for S7-1200 controller. Professional is for S7-1500 and also the "older" S7-300/400 controller. Safety Basic/Advanced is for programming FailSafe controller Startdirve is for drives. There are also some more SW-Packages possible to integrate in TIA. Have a look to the delivery release for V16: Delivery release TIA Portal V16hope this helps, regards, |
FCK WAR! |
|
Follow us on