9/9/2020 1:19 PM | |
Joined: 1/22/2014 Last visit: 8/25/2024 Posts: 39 Rating: (0) |
Dear All, I have PCS7.1 and WinCC 7.0 with ES, OS, OS(SBY), CLIENT and 8 Client Ref XP PC stations Recently one of the Client Ref PC crashed and I installed everything from scratch, Win XP SP3, WinCC Client. I used the same name and IP address for the PC as before. Then I tried to download to the Client Ref Station from the ES as usually. It starts copying the complete project and then tries to open the project. Unfortunately it is ending with 'Some error occurred and downloading was not successful' Any advice for what may be the reason of this ? Thank you, GKaim ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/09/2020 13:39:41New subject after splitting |
|
9/10/2020 8:39 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Best regards, Jen_Moderator |
Follow us on