10/15/2020 8:10 AM | |
Joined: 3/30/2020 Last visit: 4/23/2024 Posts: 4430 Rating: (925) |
Hello. What you see is in the definition of the JC instruction. See the attached PDF for the in-software HELP description. The focus sentence is..
It makes perfect sense that the line following the JUMP should have the RLO in a TRUE state. BR Attachmenthelp-jc.pdf (174 Downloads) |
Last edited by: qwazee at: 10/15/2020 08:10:36add pdf Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/15/2020 8:11 AM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046)
|
Hi dany brown it's perfectly correct what you see as the JC will set the RLO to 1 (press F1 on it and the help will tell you the same). You can think of the humble JC statement as a single STL instruction that is akin to an IF THEN ELSE high level langue construct. IF RLO is 1 THEN jump to label to continue there, ELSE set RLO to 1 and use as you see fit Your example logic is shooting itself in the foot as the JC jump destination is the next line behind the JC statement itself so instead of being an IF THEN ELSE it is more like a "always do it no matter what" |
Last edited by: fritz at: 10/15/2020 08:13:26Last edited by: fritz at: 10/15/2020 09:01:12qwazee beat me to the answer by a minute, but at least we concur Cheers |
|
This contribution was helpful to1 thankful Users |
10/15/2020 5:47 PM | |
Joined: 11/13/2015 Last visit: 2/15/2024 Posts: 24 Rating: (0) |
Hi, The pdf very helpful, now i already understand it |
This contribution was helpful to1 thankful Users |
10/15/2020 6:08 PM | |
Joined: 11/13/2015 Last visit: 2/15/2024 Posts: 24 Rating: (0) |
Perfectly, i already understand and find what issue from some rungs Many thanks |
Follow us on