1/11/2021 11:18 AM | |
Joined: 1/9/2017 Last visit: 9/18/2024 Posts: 8 Rating: (0) |
All i need gsd file for below module ET 200 PA smart 6ES76508PH000AA0 |
1/11/2021 11:38 AM | |
Joined: 1/9/2017 Last visit: 9/18/2024 Posts: 8 Rating: (0) |
Yeah i need it for pcs7 |
1/12/2021 12:35 AM | |
Joined: 10/7/2005 Last visit: 9/18/2024 Posts: 3021 Rating: (1054)
|
Hi VISSU@123 the IM650 based ET200PA SMART is a bit of a PCS7 special beast. See the manual for more and also attached excerpt to see if you have the per-requisites fulfilled. While not 100% sure, I would not all be surprised if a GSD file does not exists for it and (PCS7) HW-catalog metadata based config is the only way. |
Cheers |
|
Follow us on