1/19/2021 2:14 PM | |
Joined: 1/5/2021 Last visit: 10/5/2022 Posts: 1 Rating: (0) |
I am using ET200SP. I want to communicate with Inverter Delta C2000 by using Modbus Rs-485 Commination. I using the Modbus_Master_DB and Modbus_Comm_Load modules ET200SP----CMPtP---Modbus Rs-485---Delta Inverter C2000 a) Modbus_Master_DB: 1. MB_ADDR: 2 (I set address no 2 in inverter) 2. MODE: 1 3. DATA_ADDR: 40002 4. DATA_LEN: 1 b) Modbus_Comm_Load modules: 1. PORT: "Local~CM_PtP_1" 2. BAUD: 9600 3. PARITY: 0 However, when i send to frequency, there nothing happen happen. can someone help me what is the problem ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2021 05:52:24New subject after splitting |
|
Follow us on