1/26/2021 9:21 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello, Have a look at the following link: How do you create and update multiple instances? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
1/26/2021 9:50 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Thank you for answering Wizard, It seem to work (not that it is tested but Simatic Manager does not paint it red) when I convert the block to a multi instance block. But why does it have to be multi instance when I only plan to use it once? What can I type in at the PT pin if I want a 10s pulse each tine the IN pin it activated?
|
Follow us on