2/10/2021 3:47 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, What I always do is to have suffix (StepNr) behind the calculation like: Count total flow (S1000) where S1000 is my stepname This way, it is unique. PS: The names are only checked in a sequencer. If you have another sequencer, calling the same name, it won't be changed automatically only when using the same name in the same sequencer. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on