2/10/2021 5:18 PM | |
Joined: 3/14/2008 Last visit: 3/29/2024 Posts: 2059 Rating: (924)
|
Hi Wim, Have you seen the following FAQ: RT station not obtainable . Reinstalling should not be the solution. Usually it means something is wrong with the network or network settings. In the link are a few suggestions. Also take a look at Simatic Shell if the stations are visible or not at the time you cannot download. Maybe you can share some details about the configured setup? You can also upload the DLDownloadOS.log from the diagnose folder at the time of the error, it can be found in Program Files(x86)/SIEMENS/WinCC/diagnose. |
Last edited by: Jen_Moderator at: 02/11/2021 07:58:37Optimized link. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on