2/26/2021 10:47 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi ABCGGKK, the OS-Client license is for one Client. How many OS-Servers are connect to the OS Client is not significant. For example you have 4 OS-Clients and 3 OS-Servers, then you need 4 OS Client license and 3 OS-Server licenses, no matter how the OS-Client and OS-Server are connected. With regrads |
This contribution was helpful to1 thankful Users |
2/26/2021 11:31 AM | |
Posts: 198 Rating: (60) |
The OS Client license will be required for every individual OS client PC. It will not depend on the number of server project connections (as long as you are within the maximum limits permitted for the particular PCS7 version). It only depends on the number of clients and version of PCS7 used. For more information on the license requirements, you can refer thelicensing and configuration limits for PCS7 V8.2. Hope this helps! |
This contribution was helpful to1 thankful Users |
Follow us on