2/17/2021 5:14 PM | |
Joined: 10/10/2014 Last visit: 4/18/2024 Posts: 1725 Rating: (208) |
Hi AutoGen_6753138 What do you want to monitor ? If the stations are running ? Best regards schufri |
2/26/2021 9:04 PM | |
Joined: 9/21/2006 Last visit: 5/25/2023 Posts: 247 Rating: (61) |
If I understand the question, you are asking if there is a way to create buttons that will select the WebNavigator pages from different servers to be displayed, based on which button is pressed. Possible ways to implement this:
|
Follow us on