3/6/2021 11:32 AM | |
Posts: 2 Rating: (0) |
dear sir/madam i use s7-200 cpu 224xp i need store the product number per shift at the HMI so i use the counter c0 and connect the proxy sensor for specified input so i use the add to table instruction for store the c0 when shift is finished so vw400 and vw402 used by system and i use vw404 .... problem: when i move 99 to vw400 every thing is ok but when move number above from 100 thats not work and add-to-table not working why i can'not use the table for 500 number?? please check the attachment. thanks Attachmenthoma steel pipe counter VER3.zip (409 Downloads) |
3/6/2021 12:35 PM | |
Posts: 2 Rating: (0) |
dear duris thank you for fast reply yes. add-to-table limited by 100 so i need new way for storing the c0 counter did you have any idea for this application? |
Follow us on