3/10/2021 3:02 PM | |
Joined: 3/22/2012 Last visit: 2/26/2024 Posts: 2 Rating: (0) |
Dear Sir, I have a problem V-ASSISTANT_v1-07-00 by Ethernet Cable connection after V90 Firmware Update. Description: When The Firmware was the original firmware (V1.02.00) I was Able to go online by Ethernet Cable and by USB cable and establish a connection with a V90 After the V90 Firmware Update (to V1.04.03) i am able to connect only by the USB cable and not with the Ethernet cable. I get a error message. “Failed to Open the configurationfile. Please fix or reinstall the software” I try to reinstall V-assistant: Same Error. I try To install V-assistant in Win 10 and Win 7: Same Error Details: My V90 device is: SINAMICS V90, con PROFINET tensione di ingresso: 380-480 V 3 A - 15 %/+ 10 % 6,6 A 45-66 Hz tensione di uscita: - 0 ingresso 5,3 A 0-330 Hz motore: 1,5/1,75 kW grado di protezione: IP20 grandezza costruttiva B: 100x180x220 (LxAxP) Originally the firmware was V1.02.00 I Update The firmware to SINAMICS_V90PN_04743536_01040300.zip (10,2 MB) V-Assistant is: SINAMICS-V-ASSISTANT_v1-07-00 Can You Help Us? |
Follow us on