5/30/2008 11:35 AM | |
Posts: 3 Rating: (0) |
Can I connect a 0-10V sensor to the SM331 analog input module? When configuring this module in S7 this optin is not aviable! |
5/30/2008 2:23 PM | |
Posts: 6 Rating: (0) |
You have to check the technical information from that module, some can only measure resitant. |
5/31/2008 3:46 AM | |
Posts: 510 Rating: (117) |
The 331 modules support +/- 10 V except the RTD and TC modules What module are you using? Bill |
6/1/2008 7:46 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Could you tell us the MLFB/ Order number of the module? |
Ayman Elotaify |
|
6/2/2008 8:35 AM | |
Joined: 9/23/2005 Last visit: 4/26/2024 Posts: 4522 Rating: (698) |
On some modules configuration is done by means of coding devices placed on the side of the module (black squares). And you cannot do it in HWConfig. Refer tothis manual please. |
Regards, |
|
Follow us on