Industry Online Support
Technical Forum
11/30/2009 6:26 AM | |
Posts: 9 Rating: (0) |
i have sinamics S120 with CU320 control unit , i want to communicate through MPI adapter , ( one end MPI/DP & another end USB ) , i have MPI adapter version 1.3 with this can igo 1.5Mbps speed ? what i have to elect in PG/PC interface access point of application either MPI ( auto) , MPI (profibus) ? actually i don't have sinamics CU320right now so that i can test , I have one litareture regarding USB adaptor ( you can find in attachment ), but is it possible with V1.3 MPI adaptor to achive 1.5 Mbps speed? pls. let me know it's very important for us. Regards, SP77 AttachmentNote on using USB PC Adapter.pdf (370 Downloads) |
11/30/2009 6:44 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, If we are speaking about 6ES7972-0CB20-0XA0 USB PC adapterfirmware V1.3, from PC Adapter USB manual(Chapter 6.1) said:
With regards, Hristo Mihalev |