7/8/2020 9:40 PM | |
Posts: 4 Rating: (0) |
Well, since I appear to be talking to myself I guess I will tell myself the solution I have found... Setting my COUPDEF from (S2,S1,-1,1,"IPO","DV”) to (S2,S1,-1,1,"COURSE","DV”) seems to have solved the issue. I am now able to run through the program in it's entirety. I was also able to find the variables that set the tolerances for FINE and COURSE types. There is a position tolerance and a velocity tolerance. Mine are set to: MD37200 COUPLE_POS_TOL_COURSE - Position Course:0.0393" MD37210 COUPLE_POS_TOL_FINE - Position Fine:0.0196" MD37220 COUPLE_VELO_TOL_COURSE - Velocity Course:2.362 in/min MD37220 COUPLE_VELO_TOL_FINE - Velocity Fine:1.181 in/min This is the best reference I have found for the information related to the coupling definition: https://cache.industry.siemens.com/dl/files/510/56950510/att_53967/v1/FB2_0911_en_en-US.pdf |
Last edited by: tome9999 at: 07/08/2020 21:42:03 |
|
This contribution was helpful to1 thankful Users |