(1)| 1/12/2014 1:27 PM | |
|
Joined: 9/27/2006 Last visit: 1/12/2026 Posts: 12480 Rating:
|
Hello Peter; The 20-750-ENETR is an Ethernet/IP comm. card for Rockwell drives, and it uses EDS files to transfer comm parameters to an Ethernet/IP processor. The S7-1200 cannot connect to the Ethernet/IP protocol directly over its Ethernet ports. You would need an external gateway to connect the S7-1200 to ethernet/IP. S7-1200 is a Profinet IO controller on its integrated ports, and the Powerflex does have a Profinet option: PowerFlex 20-750-PNET Profinet Single-port Option Module The S7-1200 can alsobe a Profibus-DP master, if you use the CM 1243-5 module, and use the GSD file provided by Rockwell along with a Profibus slave adapter: PowerFlex 20-750-PBUS Profibus DPV1 Option Hopw this helps, Daniel Chartier |
| 1/12/2014 3:03 PM | |
|
Joined: 9/16/2013 Last visit: 2/26/2025 Posts: 51 Rating:
|
Hello dchartier Thank you for the information, it has helped a lot Kind regards Peter |
Follow us on