(1)| 4/21/2014 9:28 AM | |
|
Posts: 3 Rating:
|
Hello, I am using the MD720-3 Gsm module i tried it with hyperterminal it works.I also tried it with plc,but there is some problem.According to the program i get the modem initialisation & sms send bit true,but the sms is not being send. I tried the following process: 1.allocation of Message_no to texts & TelNo.I entered the smsc no & tel no. 2.initialize modem & send sms variable via vat table. 3.i also monitered the scl block, same result "sms send=true" 4.I am using 32byte ascii module. 5. i also checked the wiring between gsm module & ascii module from the following manual below. PFA. Help me if it's possible
Attachment25545680_Application_SMS_MD720-3_DOKU_V2_1_en.pdf (104 Downloads) |
| 5/17/2016 11:34 AM | |
|
Posts: 4757 Rating:
|
New question published by sepehr.hsn is split to a separate thread with the subject How can i access to signal strength of MD720-3?. Best regards |
Follow us on