3/21/2014 9:30 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22223 Rating: (2979)
|
Hello, if you don't know which FW Version is exactly used in the drives you should use the Starter. The actual Version you can download here. 1) on the CU310 the parameters stored on the CF Card in the CU 2) on the CU240 the parameters stored on the builtin memory of the CU 3) if you Adapter have PROFIBUS support the you can use it, which Adapter have you exactly? 4) yes you can upload all connected drives insteed of cennecting each drive seperatly Regards Christoph |
3/21/2014 1:18 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
ok i wil try with tese methods ! On the first attached Photo_02, the green cables are not for Profinet connection ? |
3/21/2014 1:28 PM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22223 Rating: (2979)
|
hi, no this green cables look like sensor or DI/DO signals. Regards Christoph |
3/21/2014 1:58 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Dear Christoph, thank you very much for your advice. I'll try the methods ! Thanks again ! |
Follow us on